Part Number: SN65LVDS4SN65LVDS4: BXL tool is not creating a 3D file
Does anyone a 3D step file of this device? Does anyone suffering the same behaviour a proper solution?
Thanks in advance
Hi Rajesh,
We offer a three LVDS receiver options with integrated level shifting: DS90LVRA2, DS90LVRA2-Q1, and SN65LVDS4.
Please refer to these application notes:
How to Use a 3.3-V LVDS Buffer as a Low-Voltage LVDS Driver (ti.com)
How to Support 1.8-V…
Part Number: SN65LVDS4 Hello,
Datasheet of this part states that VCC should be powered up before VDD or at the same time for proper device operation.
Could you please elaborate proper device operation? Would it just take more current, it will damage the…
Part Number: SN65LVDS4 Hello Team,
Can you share additional information on the noise floor and phase noise of the SN65LVDS4 beside the info of the datasheet?
While not verified in production, it might be handy to have additional information as reference…
Part Number: SN65LVDS4 Hello Team,
do you see any problem if between the FPGA and the SN65LVDS4 only one 100ohm resistor is used?
In particular the 100ohm resistor is closer to the SN65LVDS4 rather than the FPGA.
I would say that the trade off might be…
Part Number: SN65LVDS4SN65LVDS4RSET --
datasheet has typical and max spec for propagation delay time. What is the min propagation delay time spec?
Thanks.
Part Number: SN65LVDS4 Hello Team,
do you have specific recommendations for SN65LVDS4 layout and bypass capacitor/s and filtering on the input, to minimize the noise floor and phase noise?
Please share also the capacitor type you would recommend.
Do…
Part Number: SN65LVDS4 Hi team,
my customer take LMK05805 clock output (122.88MHz) as the SN65LVDS4 input, shown as below. In this way, the input is AC coupled and the voltage swing (VOH-VOL) is about 500~800mV. Could you please help to check whether…
Part Number: SN65LVDS4 Hi,
I know the standard VCM for LVDS is 1.2V. However my driver has an output VCM spec of min 0.8V. I'm using the SN65LVDS4 with VCC=1.8V. Will the SN65LVDS4 properly recover the input with this low VCM? Note that I'm using the…