Part Number: SN65LVDS93 Tool/software: We are going to use sn65lvds93dgg in our design. Our plan is to use 3-channel only instead of 4-channel. Can we use it. Do we need to terminate inputs by pull-up and also any registers need to configured and what…
Part Number: TFP401 Other Parts Discussed in Thread: SN65LVDS93B , DS90C387A , Tool/software: Hi everyone,
I have an issue I’d like to clarify. Due to the temperature constraints (my requirement is that the components must operate between -40°C and…
Part Number: SN65LVDS93 Hi Team,
My customer is finding the transmitter which can support 1080p display, may I confirm if SN65LVDS93 can support 1080p resolution?
BTW, what's the highest resolution that SN65LVDS93 / SN65LVDS93A / SN65LVDS93B can support…
Part Number: SN65LVDS93 Hi,
can I use an FPGA with 2.5V logic level (Voh=Vdd-0.2V), were VDD=2.5V+-5% , for all temperature ranges?
according to the datasheet , Vih=2V, and from the FPGA my worst case scenario is 2.5V*0.95-0.2V=2.175V (typical will…
Part Number: SN65LVDS93 Do we need pullup resistors for Data input lines?
section 7.5 Electrical Characteristics in datasheet says " Rpdn Input pulldown integrated resistor on all inputs (Dx, CLKSEL, SHTDN, CLKIN) of 100k if IOVCC is 3.3V. but in "Figure…
Part Number: SN65LVDS93 Hi,
we are using two 15.1inch display panels, one is from innolux and the other one is from highness,
we are using custom board with stm32f476 mcu with 16bit rgb to lvds interface, for rgb to lvds conversion we use sn65lvds93…
Part Number: SN65LVDS93 Hi Team,
For SN65LVDS93 A version and non-A version, I assume that they are p2p compatible. The main difference is PCLK spec. Our application PCLK = 55MHz, I think we can use both of them. But when we used non-A version, the…
Part Number: SN65LVDS93 Hi Sir,
May I learn from you SN65LVDS93 INPUT channel(Dn) status will keep High or Low level if I didn't apply supply voltage to the IC?
Can you kindly let me know the status of INPUT channel(Dn) with and without VDD?
Thank…
Part Number: SN65LVDS93 I need to input 16 bit RGB data to the SN65LVDS93 to get LVDS on the output, can someone tell me which RGB signals go to which data pins to allow this on the SN65LVDS93?