Part Number: SN65LVDS93A-Q1 Other Parts Discussed in Thread: SN65LVDS94 , SN65LVDS93A Hi TI team,
We are using SN65LVDS94 part in our project.
This part is capable to support spread spectrum and specification found from datasheet as below which is for input…
Part Number: SN65LVDS93A-Q1 Other Parts Discussed in Thread: DS90CF383B , , SN65LVDS93B-Q1 Hi, TI expert
The customer was using DS90CF383MTD, but was looking for a replacement due to discontinuation.
So, DS90CF383B was recommended, but the operating temperature…
Part Number: SN65LVDS93A-Q1 Hi Sirs
From Datasheet Table 2. Pixel Data Assignment, there are 3 different formats for 8 bit connection.
My question is, if processor use format-1 (R0 to D0, R1 to D1, etc.), what kind of scheme can inform LVDS display of now…
Part Number: SN65LVDS93A-Q1 Hi Team,
Our actual air temperature is below 80°C, and the temperature of the board is 96°C,
but the junction temperature of the chip is calculated to be less than 100°C. Can the chip work in this way?
Th…
Part Number: SN65LVDS93A-Q1 Hi team,
My customer has been looking for the alternative of SN65LVDS93A-Q1. Do we have it? My customer doesn't want to degrade the data rate.
Hopefully, SEP version of SN65LVDS93A-Q1 is needed. Do we have it?
Best regards…
Part Number: SN65LVDS93A-Q1 Other Parts Discussed in Thread: SN65LVDS93A , SN65LVDS93 Hi team,
Due to some shortage, my customer want to replace SN65LVDS93AIDGGRQ1 with SN65LVDS93DGGR
is it a drop in replacement? any suggestions for this case?
BR
Fanb…
Part Number: SN65LVDS93A Team,
My customer is looking to replace the SN65LVDS93A with the Q1 version. When comparing SN65LVDS93ADGGR with SN65LVDS93AIDGGRQ1, there are some differences:
SN65LVDS93A-Q1 has worse thermal properties.
Different ESD standards…
Part Number: SN65LVDS93A-Q1 Hello,
I have a question below on the SN65LVDS93A-Q1.
In section 6.5 there is an Electrical Characteristic parameter called “delta |VOD|- Change in the steady-state differential output voltage magnitude between opposite binary…
Hi Swami,
SN65LVDS93A-Q1 FlatLink Transmitter datasheet (Rev. B) (ti.com)
This option has the 3.3V, Open-air operating temperature range goes to 85 C, but the frequency is limited to 10 - 135 MHz.
The DS90C383B only has a frequency range from 18 to 68 MHz…
Part Number: TFP401A-Q1 Other Parts Discussed in Thread: SN65LVDS93A-Q1 Hi team,
May we use the TFP401A-Q1 + SN65LVDS93A-Q1 to achieve HDMI to 2port LVDS? Resolution is 2400*900*60(frame rate)
I have suggested 949+948.
Roy