Hi Paul,
Paul Shaffer said: Question 1: Have any ESD failures for the Serial-DeSerial IC TI part number SN65LVDS96? If yes, what were the failure modes? Are there any CRC errors during the ESD tests?
ESD events that are below the listed ESD limits will…
Part Number: SN65LVDS95 Team,
Customer is looking to add SN65LVDS95DGGR to the AVL, and the device they are using today has 3.3V applied to pin 14 which we label NC. Is it allowed to have pin 14 connected to 3.3V?
Thank you!
Part Number: SN65LVDS95 Other Parts Discussed in Thread: SN65LVDS96 These pins are shown in the pin map of the IC, but not mentioned anywhere else. We've been using this chip for years with a LC filter on each pin, but the datasheet says nothing about…
Part Number: SN65LVDS95 Tool/software: WEBENCH® Design Tools I am looking for a circuit schematic of the SN65LVDS95 evaluation kit. Are unused inputs simply grounded?
Part Number: SN65LVDS95-EP Dear TI experts,
Im interested in 'SN65LVDS95DGGR- EP'.
There are 2 options,
1) SN65LVDS95DGGREP
2) V62/04643-01XE
what is different between those parts?
Their price is same/ spcification seems same
Are they implment…
Part Number: SN65LVDS95 Other Parts Discussed in Thread: SN65HVD233 , SN65HVD233-EP , SN65HVD233-Q1 Dear TI experts,
Im sooyeon Lee working in Satrec Initiative.
Our company have some heritage of the SN65LVDS95 without any option such as Q1 or EP.
But…
Part Number: SN65LVDS95 Hi,
Can you help me understand the ESD classes on the aforementioned part. The Abs Max chart list the following…
I have a few questions.
1) What is Class 2B? Is this a typo? Should it say 1B? 883 does not have a 2B…
Hi,
I'd like to understand more about t7
1) t7 (delay time CLKIN and CLKOUT) is derived? What are the factors affecting it? What is the min and max value?
2) What are the variations of t7 between different devices under same conditions and input signal…