Part Number: SN65LVDT125A Other Parts Discussed in Thread: SN65LVDS125A Hello Team, We are planning to use the IC SN65LVDT125A in one of our products. The use case seems little differnt from the intended application of the IC.
We have an MCU which acts…
Part Number: SN65LVDT125A Hi,
I am looking to create an LVDS multiplexer to switch 6 devices under test (8 pairs each) to 1 acquisition card. 7 pairs are outputs from the DUT, 1 pair in an input to the DUT.
The signalling rate is <75Mbps. The data…
Part Number: SN65LVDT125A Hello,
I have a question about SN65LVDT125A.
[Q]
Can I left be open the unused input terminal?
I think it's okay because of fail-safe.
Best Regards,
Kaede Kudo
Dear Team
My customer would like to use SN65LVDT125 for cross point switch, and i would like to know the difference between 125 and 125A, and which do you prefered, thanks.
Other Parts Discussed in Thread: SN65LVDT125A Hi all,
Are there are LVDS 4x4 Crosspoint switches like SN65LVDT125A that are failsafe.
In the data sheet it says nothing about failsafe on the LVDS inputs. Is it failsafe? If yes, in which modes?
If…