Part Number: SN65LVDT390 Other Parts Discussed in Thread: TXU0104 , SN65LVDS4 , DS90LVRA2 I have a query which is I mentioned below
1. I need connect LVDS single ended signals from SN65LVDT390PW this LVDS driver to M2S060-FGG676I Bank 8 and bank 1 …
Part Number: SN65LVDT390 the datasheet doesn’t state Operating junction temperature, TJ for the following devices. Please provide
SN65LVDT390PW
SN65LVDS391-01
Part Number: SN65LVDT390
Hi Team,
According to data sheet Maximum Recommended Operating Speeds is 200 Mbps. Is there a margin to some extent if the signal is a little higher than 200 Mbps?
Beat Regards, Tom Liu
Part Number: SN65LVDT390 Hi team,
I think the unit of thermal resistance in the datasheet (8.4 Thermal Information, page 8) is wrong,
it should be C/mW, not mW/°C.
My customer would like to confirm the unit in the below thread, the unit should be…
Part Number: SN65LVDT390 Hi team,
We are using the Part SN65LVDT390PWR.
The thermal data for Package Drawing "PW" is not available in Data sheet.
Please Provide The Following data for the same.
RθJA,
RθJC
and Tj Maximum
Regards
Karthik…
Part Number: SN65LVDT390 Hi Team, I hope you can help us fill in this information for our customer.
Theta Jb, Theta Jc (Top), Theta Jc (Bottom), Theta Ja, Reliability Tj Max, "Operating Tj Max", "Absolute Tj Max"
Thank you very much
Regards…
Part Number: SN65LVDT390 Other Parts Discussed in Thread: SN65LVDT390 Hi,
I am using SN65LVDT390 part in my design. The IC datasheet says it is a LVDS receiver IC for signals of data rate upto 250 Mbps.
Can we use it for LVDS clock signals of frequency…
Hello,
The SN65LVDT390 has higher ESD rating (15kV vs. 4kV for SN75LVDT390), so that's one option. If that's not enough protection then using an external ESD protection device would help. This System-Level ESD Protection Guide has more details, including…
Dear Sir,
WE are doing SI Analysis for our PCB. We are using SN65LVDT386ADBT, SN65LVDT388A,
SN65LVDT390.
IBIS model for these 3 parts does not include 100E internal termination.
Please confirm on this whether we need to provide 100E external 100E resistor…