Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: SN65MLVD201 Dears,
quick question about SN65MVLD201,
What is the unit load of SN65MLVD201? or what's the maximum bus nodes of this device?
currently we found 16nodes bus cannot support 25Mbps in our real system. so we ask this question…
Other Parts Discussed in Thread: MLVD20XEVM , SN65MLVD201 , THVD1450 , SN65LVDS050 Hi TI,
Newer engineer here, I have a 1PPS signal that will be provided via LVDS signal standard but is required to be sent to the receiver as a RS-422 compliant signal. Does…
Part Number: SN65MLVD201
For the part configuration: SN65MLVD201. I need to know the junction to case thermal resistance (Theta_JC) to the bottom of the case. I am unable to locate this information in the datasheet. Could you please provide this number…
Beyond the DC loading, both of these configurations are full of transmission line segments. The MLVDS transmit waveform will react to the transmission line impedances and the DC load of the termination resistor. To help debug this type of application…
Part Number: SN65MLVD201
Hello, I am using the 65MLVD201 MLVDS transceiver in two applications
Application 1)
I have 4 backplane connected cards in which one card has an always enabled 65MLVD201 driver driving a MLVDS pair and 3 cards have 65MLVD201…
Hello Fernando,
Thank you for your post and we again apologize for any inconvenience this brings. This model is currently in our design queue, however, since this queue also includes new releases as well as other remodels, we cannot say at the moment…
Other Parts Discussed in Thread: SN65MLVD201 Hi,
Iam designing a data acquisition system which has multiple data acquisition modules separated by a distance of upto 10 metres. I intend to send the sampling clock from one of the DAQ modules to others in…
Dear Michael-san
Thank you for reply.
Customer will use SN65MLVD201 or SN65MLVD206.
Data speed is 50MHz
※Customer hope Bi-Directional line.
(Only data line and VCC/GND, non-enable control)
If impossible, A customer will consents it.
Best regards…