Part Number: SN65MLVD204A Dear TI engineer
Please provide information on an inexpensive microcontroller to connect the SN65MLVD204A to.
Serial communication interface 3port
SPI 2port
ADC 1port
UART 1port
I2C 2port
The SN65MLVD204A uses a…
Part Number: SN65MLVD204A Hello,
I see the maximum operating temperature for SN65MLVD204ADR1G4 on the datasheet as 85C. Is the max junction temperature known?
Part Number: SN65MLVD204A Hello
If two connected SN65MLVD204A both become DE=Hi, (If data collides) Can SN65MLVD204A malfunction?
D=H.L Will it malfunction if different values are output?
Part Number: SN65MLVD204A Tool/software: Dear Technical Support Team,
When input the clock to the SN65MLVD204A, is it possible to change jitter(tjit(pp))?
Driver spec on "9 Switching Characteristics" describes 55ps(TYP)、 150ps(MAX).
For example…
Part Number: SN65MLVD204A 10.2.2.7 Receiver Input Threshold (Failsafe) Measured to confirm that it is as specified. A FET probe was used to measure the differential output.
If the -A and -B terminals are shorted together, will this kind of failure mode…
Part Number: SN65MLVD204A About SN65MLVD204AD As shown on the left The 7th pin (B) of IC39 is To pin 6 (A) of IC11, The 6th pin (A) of IC39 is I accidentally connected it to pin 7 (B) of IC11. Both IC39 and IC11 failed. *The red part is the cable between…
Part Number: SN65MLVD204A Other Parts Discussed in Thread: SN65MLVD200A Hi,
I would like to know if all parts with a same package in the family SN65MLVD20xA (so SOIC 8 on one side SOIC14 on the other side) are packaged the same way in Aguascalientes…
Part Number: SN65MLVD204A Dear team,
Customer would like to use the SN65MLVD204A driver (on the transmitter side, single-ended signal on its D input, supplied with 3.3V) to an IC which has an LVDS input.
In order to adapt the M-LVDS output of the…
Part Number: SN65MLVD204A Hi team,
My customer is asking what is the difference of SN65MLVD204A and SN65MLVD204? Why we develop SN65MLVD204A? Thanks.
BR,
CL