Other Parts Discussed in Thread: SN65MLVD206 Hi dear experts,
My customers want to confirm whether SN65MLVD206 supports hot swapable function?
Plus, if input/output pins are present before VCC powers up, will this impact device?
thanks a lot!
…
Part Number: SN65MLVD206 HI Dear expert,
How many nodes could this SN65MLVD206 support? i.e. How many LVDS could it drive? can it drive 16 LVDS?
thanks very much for your reply.
thanks!
Joyce
Other Parts Discussed in Thread: SN65MLVD206 Hi all Would you mind if we ask SN65MLVD206? Our customer plans to use the plural SN65MLVD206s. So, in this case, is maximum skew max1ns which shows on the datasheet "Part-to-part"? Kind regards, Hirotaka …
Part Number: DS25CP102 Other Parts Discussed in Thread: SN65MLVD206 , DS25CP104A Tool/software: Dear Team,
I am currently facing an issue when attempting to configure the ds25cp102.ibs file within the ADS simulation software.
Specifically, when…
Part Number: SN65LVDS31 Other Parts Discussed in Thread: SN65MLVD206 , , DS90LV032A , DS90LV031A Hi team,
My customer previously is using SN65MLVD206 & DS90LV032 in backplane MLVDS bus application.
Now they want to employ SN65LVDS31 or DS90LV031 as…
Part Number: DS91D176 Other Parts Discussed in Thread: SN65MLVD206 Hi dear supporting team,
in DS91C/D176 d/s, the true table shows the chip either be sending or receiving. while checked with SN65MLVD206 BU, it could be sending and receiving in the…
Hello Yue,
MLVDS is a good option for this application. Do they need 4 channels? If so, then DS91M040 is an option. If they only need 1 channel, then SN65MLVD206 is a good option. How many devices will be on the bus, is it just the 2 FPGAs? If that…
Hi,
I can’t locate the 32 nodes simulation data on SN65MLVD082. There is a full load simulation at 100Mbps data on full 19 slots on SN65MLVD206 and SN65MLVD200. This is somehow close to your system requirement.
The 19 nodes data shows good margin…
Other Parts Discussed in Thread: SN65MLVD206 , AM3359 , DS92LV16 Hi all.
I'm developing an industrial FPGA interconnect back plane. I need to communicate over a single differential lane, with a master that initiates a request and one out of several…