Part Number: SN74AHC1G00 Tool/software: Hi team,
My customer is using SN74AHC1G00DCKR for logic function and met wrong VIH threshould.
Issue: They connect pinA and pinB together and when input signal is up to 1.1V and then output will down to 0V.…
Part Number: SN74AHC1G00 Tool/software: Hi team,
If Vcc=5.5V, VIH=3.85V ,VIL=1.65. If Vcc=5V, Input signal ranging from 1.65V~3.85V, what would Vout status be like?
Part Number: SN74AHC1G00-Q1 Other Parts Discussed in Thread: SN74LVC1G98-Q1 Tool/software: Hello team,
A customer is asking if SN75AHC1G00-Q1 can be supported for VCC=1.8V.
Can you confirm it?
Thanks and regards,
Sam Lee
Part Number: SN74AHC1G00-Q1 Tool/software: Hi Team,
As we are performing the Functional safety analysis, we require few details related to one your part number ( SN74AHC1G00QDCKRQ1 )
Failure modes
FIT rate
Failure distribution
Please provide…
Part Number: SN74AHC1G00-Q1 Tool/software: Hello experts,
is the Spice model on ti.com from SN74AHC1G00-Q1 compatible with LTSpice?
Thanks and best regards,
Michael
Part Number: SN74AHC1G00-Q1 Tool/software: Hi experts,
does the SN74AHC1G00-Q1 have ESD protection diodes at the input pins towards the supply and GND? How is ESD protection ensured with this device?
Thanks and best regards,
Michael
Part Number: SN74AHC1G00 Tool/software: Hi, expert:
Could you tell me if SN74AHC1G00 VCC=0, what's the output state when input A and B is normal.Thanks!
Part Number: SN74AHC1G00 Other Parts Discussed in Thread: SN74LVC1G14 Hi team,
Do we have the pin2pin device with Ioff function better than SN74AHC1G00DCKR?
Part Number: SN74AHC1G00-Q1 Tool/software: Hi,
I need to know the conditions considered for measuring the Rthja of "SN74AHC1G00QDCKRQ1"
Board type used (is it FR4)
Copper thickness of board in oz
Pad layout: is it minimum recommended pad la…