Part Number: SN74AHC1G08 Hi,
We use the SN74AHC1G08DR on the circuit for sleep wake-up, and SN74AHC1G08DR is failure which the datecode is after with 2514, we consider if TI has some wafer design updated, and it is not updated in the datasheet, so please…
Part Number: SN74AHC1G08-Q1 Hi,
Customer found the output will be high when one input is 2.65V with Vcc=5.0V. The value-VIH in datasheet is 3.85V @5.5Vcc. How to explain this issue?
Thanks a lot!
Andy
Part Number: SN74AHC1G08 Hi Team,
The client wanted to get item SN74AHC1G08DBVR. According to the data sheet, the following marking options are : A083, A08G, A08J, A08L, A08S The item the client received is marked as 3BVF which they cannot use. Please…
Part Number: SN74AHC1G08-Q1 Hi Expert,
Why is the output voltage higher when Ioh=-50mA is higher than when Ioh=-4mA? Isn't this just referring to the output current at the pin?
As I understand it, when the current demand for Id is relatively small…
Part Number: SN74AHC1G08 Hi Team,
Please help to advise if the X-ray will impact the SN74AHC1G08DRLR and SN74AHC1G86DRLR quality and performance or not?
Customer worried about it once they use X-ray for IC examination.
Thanks.
Part Number: SN74AHC1G08 Hi TI,
Is there any differences between body marking AEJ with 1B9?
I am having a failure in In-circuit testing for board mounted with SN74AHC1G08DCKR body marking 1B9.
When replaced with SN74AHC1G08DCKR body marking AEJ…
Part Number: SN74AHC1G08-Q1 Hi, can you please provide
1)tpd min typ max value at 5V , 25°C ,85°C ,125°C
2)tplh min typ max value at 5V , 25°C ,85°C ,125°C
3)tphl min typ max value at 5V , 25°C ,85°C ,125°C
Part Number: SN74AHC1G08 Tool/software: Hi Texas instrument team for part number SN74AHC1G08DCKR has the mark "AEJ", can you let me know if one of these letters are related to Date Code or Just to the part number. Thank you in advance for your prompt…
Part Number: SN74AHC1G08-Q1 Tool/software: Hello All,
Any updates on the below request!
Please resubmit the IMDS (as per IMDS Recommendation) for the following part number at the earliest possible. Please resubmit it on priority. Please resubmit…