Part Number: SN74AHC1G09 Hi Team, May I ask for help? My customer have a concern as stated below:
"For SN74AHC1G09DCKR can you please provide theta JB or JC to bottom of case and maximum operational junction temperature. Datasheet only provides Tambient…
Part Number: SN74AHC1G09 Hi Team, We're aware that the max junction temperature for standard logic devices are the same as their max storage temperature, which is typically 150C as discussed on the FAQ: https://e2e.ti.com/support/logic-group/logic/f/logic…
Part Number: SN74AHC1G09 Other Parts Discussed in Thread: SN74AS808B , SN74AHC08 , SN74HC21 Hello
Is there a bigger AND gate component with more inputs than SN74AHC1G09?
I'd like to AND together up to 16 signals, but in a signal package. Using SN74AHC1G09…
Part Number: SN74AHC1G09 hello,
We are using this part in our design. This IC has power supply of 3.3V and output load current is 2.4mA.What is the VOL value for this condition please provide or else provide graph of having output voltage w.r.t. output…
Part Number: SN74AHC1G09 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Two questions:
1) is there a TINA spice model available for SN74AHC1G09
2) are there similar components as SN74AHC1G09 with more logic inputs…
Part Number: SN74AHC1G09 Other Parts Discussed in Thread: SN74AHC05 Dear Support,
I would like to have the IBIS model for the part SN74AHC1G09DBVR.
Regards,
Ahmed.
Part Number: SN74AHC1G09 All,
I have a question about function table, if two inputs are LOW, what's output? it should be high or low??
From page 1, there is a statement Y = A*B or Y = #(A+B), which means output HIGH, if A=B = LOW.
what's the output…
Part Number: SN74AHC1G09 Dear Sir / Madam,
In datasheet of SN74AHC1G09DBVR, VOL (max.) has been mentioned as 0.44V under the test condition of, IOL = 4mA, TA = –40°C to +85°C @ VCC = 3V. In our circuit we are using it at IOL = 2.27mA and i want to know…
Part Number: SN74AHC1G09 We have an existing design that has been used for 20 years and is being updated with parts that are specified from the vendor to operate from -55 °C to +125 °C. We would like to replace the parts with the exact same footprint…