Part Number: SN74AHC1G125 Other Parts Discussed in Thread: LM98725 , Hi team,
Our customer is observing differences in the electrical behavior of the SN74AHC1G125 output connected to the LM98725 following PCN 20250827001.1. Specifically, the overshoot…
Part Number: SN74AHC1G125 Hello,
I have the following requirement for a project:
A battery-buffered 3.3 V logic signal needs to be connected to a processor input.
If I were to connect the signal directly, when the processor is not powered, the internal…
Part Number: SN74AHC1G125
Dear TI Support Team,
We are using the SN74AHC1G125DBVR device in our production boards. In your previous response, you confirmed that the device marking “39HH” corresponds to this part number.
However, the ICs we require…
Part Number: SN74AHC1G125 Tool/software: Hi team,
My customer has 2 questions:
1) Current output Low and High Abs Max ratings vs. Recommended seems quite high. ±25mA vs ±8mA. Why or what causes it.
2) They use 2 buffers in series: Do we recommend…
Part Number: SN74AHC1G125 Hi TI Team,
I experiencing a functional issue with the SN74AHC1G125DCKR used as a buffer on an SPI Chip Select (CS) line.
Observations:
The issue occurs consistently with units marked "1RB".
Units marked "AMJ" function…
Part Number: SN74AHC1G125 Tool/software: Hi,
Could you highlight the difference for me between these two devices?
I assumed they are the same part with ordering through tape vs. reel, however, TI.com notes the R version as one with upgraded functionality…
Part Number: SN74AHC1G125 Tool/software: I’m having a little bit of trouble translating the exact change that is happening to the device mentioned in the subject line. It seems like there was an additionally Fab site qualified, as well as changes to the…
Part Number: SN74AHC1G125-Q1 Other Parts Discussed in Thread: SN54AHC244-SP Tool/software: Hello experts,
We want to use SN74AHC1G125-Q1 to the satellite project.
Are there any restrictions on using it on satellites?
Best regards,
Toru Kimura…