Part Number: SN74AHC1G32 Other Parts Discussed in Thread: SN74LVC1G07 Hi,
Is SN74AHC1G32 an open-drain output OR gate? If not, do we have any open drain output OR gate?
Thanks!
Antony
Part Number: SN74AHC1G32 Hi,
Datasheet of this logic shows that this device has "Schmitt-Trigger Action" at top page. But "Input transition rise and fall rate" are described in datasheet of page 4.
Is this logic supported Schmitt-Trigger? and what…
Other Parts Discussed in Thread: SN74AHC1G32 , SN74LVC1G97 Hi,
My customer are looking for an OR Gate which integrate Schmitt-Trigger.
SN74AHC1G32 mention about the Schmitt-Trigger Action.
But is there a Schmitt-Trigger inside? Or just use other…
Other Parts Discussed in Thread: ADS1675 , SN74AHC1G32 , SN74AHCT1G32 Hello,
i've built a pcb based on ADS1675REF board.
Actually board does not behave the way i was expecting, analyzing signals on PCB to see if something's wrong i've discovered that…
Part Number: SN74AHC1G08-Q1 Other Parts Discussed in Thread: SN74AHC1G32 What is the typical Response Time vs Output Voltage for SN74AHC1G08-Q1 family?
Reposting the list of devices with GPNs as the answers wont change between package types or quantity
SN74AC74 SN74AHC1G32 SN74AUP1G99 SN74LVC04A SN74LVC04APWTE4
SN74LVC125A
SN74LVC126A
SN74LVC1G07
SN74LVC1G08
SN74LVC1G14
SN74LVC1G97
SN74LVC1G99…
Part Number: TPS2521 Other Parts Discussed in Thread: SN74AHC1G02 , SN74AHC1G32 Hi all,
i have set the UVLO limit on TPS25210ARPW to 4.5V like so:
and i want to drive the EN pin from external NOR SN74AHC1G02 gates ( push-pull output) like
…
Part Number: SN74AUC1G32 Other Parts Discussed in Thread: SN74LVC1G32 , SN74AUP1G32 , SN74AHC1G32 , SN74AUP1T32 , SN74LV1T32 Hi Team,
I see that this device can have a Vcc of up to 3.6V.
for the logic input the recommended operation is 2.7V (Vcc)…
Hello Malcolm-san,
I got their reply which states their system requires and show those in the attached. Would you please check the attached and give me your comments and input your suggestion if you have?
CD4027B_Alternatives_2024July12.pptx
Best…