Part Number: SN74AHC595 Other Parts Discussed in Thread: SN74AHC74 Hi Team,
Where can I get IBIS model of SN74AHC595? I didn't find that on the website.
Thank you.
Part Number: SN74AHC595 Hi team,
Because the SRCLK and the RCLK is the positive edged triggered.
Does it triggered in 50% of the edge? The customer want to know the exact voltage for the clk to sample the data.
Do you have the CLK voltage to sample the…
Part Number: SN74AHC595 Other Parts Discussed in Thread: TCA6408A ,
Hello
My customer is looking for high-speed I/O expander.
They are using TCA6408A already in the other product, and they know it well , but i2C is 400Ksps and very slow.
Customer need…
Part Number: SN74AHC595 Hi, team,
I have two questions about SN74AHC595 may need your help.
What is the recommended max VIH when VCC is 5V/3V/2V?
What is the recommended VIH min and max voltage when VCC=3.3V?
Thanks.
Johnny
Part Number: SN74AHC595-Q1 Hi,
We are using a SN74AHC595-Q1 in a design and have some questions about the input voltage tolerance and current on the shift register SER input. We’re powering the device with 2.5V and we need to drive the serial input with…
Part Number: SN74AHC595 Other Parts Discussed in Thread: SN74AHCT595 Hi,
There are two types of devices SN74AHC595 and SN74AHCT595.
Can anyone explain the difference of these two devices?
I'm reviewing datasheets, and cannot find anything until now.…
Part Number: SN74AHC595 Hi Sirs,
Sorry to bother you.
We have use SN74AHC595 to replace NXP 74AHC595.
Schematic as below
The SH-PoE’s LED is random display during manual reset.
MR=SN74AHC595 SRCLR
But can normal display after manual reset.
Our…
Other Parts Discussed in Thread: SN74AHC595 , SN74HC132 Hi there,
I'm new to these forums, so I hope I'm posting in the right section. First off, this question is regarding datasheet information only at this point--no testing has been done to confirm/discount…
Hi there,
I'm new to these forums, so I hope I'm posting in the right section. First off, this question is regarding datasheet information only at this point--no testing has been done to confirm/discount the Electrical Characteristics I'll refer to.…
Part Number: SN74HCS595 Other Parts Discussed in Thread: SN74AHC595 Dear Team,
Do we have comparison table of NEXPERIA 74AHC595PW and SN74HCS595PWR ?
Many Thanks,
Jimmy