Hi there,
I'm new to these forums, so I hope I'm posting in the right section. First off, this question is regarding datasheet information only at this point--no testing has been done to confirm/discount the Electrical Characteristics I'll refer to.…
Part Number: SN74HCS595 Other Parts Discussed in Thread: SN74AHC595 Dear Team,
Do we have comparison table of NEXPERIA 74AHC595PW and SN74HCS595PWR ?
Many Thanks,
Jimmy
Why have you chosen this particular device? Do you really need a bipolar, military-grade device?
As far as I can see, the '673 is not really designed for cascading. You can share all inputs, except for /CS, to address them separately.
If you have…
There are several alternate parts (SN74AHC595, SN74AHCT595, SN74HCS595, SN74HC595, SN74HCT595, CD74HC595), but all of them have outputs with lower drive strength.
Other Parts Discussed in Thread: SN74AHC595 Hi
Does anyone know if the SN74AHC595 from TI also has schmitt trigger inputs like the one from NXP?
Thanks and best regards,
Fabian
Part Number: SN74HC595 Other Parts Discussed in Thread: SN74HCS595 , SN74AHC595 , SN74LV595A Hi team,
here we want to check the output drive current in 3.3V supply.
there is only have data for 5V supply as below.
i also see it will decrease in low voltage…
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74AHC595 , Hi
I have a question to ask about the design of serial-to-parallel conversion design, which parts should be paid attention to, such as how to consider the bandwidth
There are no guaranteed electrical characteristics for any supply below 5 V.
Better use a device from a low-voltage logic family, e.g., SN74HCS595, SN74AHC595.
Part Number: SN74ABT273 Other Parts Discussed in Thread: SN74AC74-EP , SN74AHC595-Q1 , SN74HC273-Q1 , SN74HCT14-Q1 , SN74HCT244-EP Hi team, Good day.
What is the ESD HBM of the following part numbers?
SN74ABT273 SN74AC74-EP SN74AHC595-Q1 SN74HC273-Q1 SN74AC74-…