Part Number: SN74AHCT125-Q1 Tool/software: Hi team,
I found a mismatch of pin description below.
Please see below pin # 8 and #10.
Pin description of #8 and #10 pin is flipped from Figure5-1.
It looks Figure 5-1 is correct, but could you please double…
Part Number: SN74AHCT125
Hi team,
Is the TA of SN74AHCT125PW -40~125 or -40~85? It seems there is a confusion in the datasheet. sn74ahct125.pdf
Thanks & best regards,
Wendy
Part Number: SN74AHCT125 Other Parts Discussed in Thread: SN74LVC1G17 Hello and good day to all of you,
I'm Thilesh De Silva a research assistant in University of Peradeniya Sri Lanka. I'm Using SN74AHCT125N for one of my application circuits. Please…
Part Number: SN74AHCT125-Q1
Please send following graphs if you have.
1. VOH - IOH
2. VOL - IOL
Our customer need above information not only below test condition.
VOH-IOH,VOL-IOLpptx.pptx
Part Number: SN74AHCT125-Q1 Question1:
Is there protection diode (clamp diode ) in input pin ?
Question2:
When VCC=0V,Does this part accept to be applied 0V to 3.3V to input pin ?
For voltages below V IH , the input is not guaranteed to be read as high. (And worse; see [FAQ] How does a slow or floating input affect a CMOS device? )
To convert from 3.3 V to 5 V, use a device with TTL-compatible inputs, e.g., SN74HCT244 (8ch), SN74AHCT125…
AHCT devices support up to 170 Mbps.
If you need just a buffer (and not an AND gate), consider the SN74AHCT125 (or SN74LV125AT for higher drive strength). If you need fewer channels, consider the SN74AHCT1G08 or SN74AHCT1G125.