Part Number: SN74AHCT1G32 Other Parts Discussed in Thread: SN74LV1T34 Hi,
my customer uses SN74AHCT1G32DCKG with 3.3V instead of 5 V by mistake.
#20259_sn74ahct1g32.pdf
According to the attached app note:
feeding the device with only 3.3V…
Part Number: SN74AHCT1G32 Hi Support team
Customer would like to understand the state of the output pin when the device is in the process of having the power supply ramped up. Is the output high Z or if both inputs are pulled low, and there is a pull…
Part Number: SN74LVC1G32 Other Parts Discussed in Thread: SN74AHCT1G32 Tool/software: Can you confirm what state the output will be of the SN74LVC1G32 when the input is between Vil and Vih? In this application, Vcc=5V. So what are the conditions when…
Part Number: SN74AHCT1G14 Other Parts Discussed in Thread: SN74AHCT1G32 Hi, Our customer downloaded the Spice model for SN74AHCT1G14 ( http://www.ti.com/lit/zip/slcm007 however when they've opened the .zip file they see that the Spice model is for SN74AHCT1G32…
The actual switching threshold will be somewhere near V CC /2. But if an input stays in the range between 0.3 × V CC and 0.7 × V CC , the device will not operate normally because you have violated the Δt/Δv limit; see [FAQ] How does a slow or floating…
Hello Greg,
i've analyzed signals the best i can on the board and at the moment i'm focusing on clock signal delivered to ADC,
i've asked a question regarding this on the apposite section of E2E community: http://e2e.ti.com/support/logic/f/151/p…