Part Number: TXV0108 Other Parts Discussed in Thread: SN74AUC244 Tool/software: Hi team,
My customer plans to use TXV0108 for the level translation of 1.5V<->1.8V and 1.8V<->1.5V. Output channel-to-channel skew of them are not stated on the datasheet…
Part Number: TXV0108-Q1 Other Parts Discussed in Thread: SN74AUC244 , SN74AUC34 , TXV0108-EVM Tool/software: Hi,
From the datasheet this info cannot be found, please advise:
from 3.3V Port A to 1.2V Port B, is the data speed 100MHz (200Mbps) supported…
Part Number: SN74AUC1G125 Other Parts Discussed in Thread: SN74AUC2G125 , SN74AUC125 , SN74AUC244 , SN74AUP1G125 , SN74AUP2G125 Tool/software:
I find out SN74AUC1G125, a tri-state buffer with output enable that works fine at VCC=1.0V. However, the Vih…
Other Parts Discussed in Thread: SN74LVC125A , SN74AUC34 , SN74AUC244 , SN74AUC125 Dear TI,
Could you please recommend buffer/driver solution for 1.8V JTAG bus?
Thanks
Part Number: SN74ALVC244 Other Parts Discussed in Thread: SN74AUC244 , SN74LV244A , SN74LVC244A , SN74LVC541A
Tool/software:
Hi,
I'm using the buffer SN74ALVC244 to drive some other IC input pins on an existing PCB.
The IC is already active before…
Part Number: SN74LVC244A Other Parts Discussed in Thread: SN74AUC244 , Hi Sir,
Did we have any bi-direction buffer/line-driver solution for SD card application which the function same as the SN74LVC244A or SN74AUC244?
Thanks,
George
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74AUC244 Hello
SN74AVC16T245 an support 80MHz clock signal. From B -> To A
VCCA=1.8V
VCCB=2.5V
Thanks
Roi
Part Number: SN74AVC8T245 Other Parts Discussed in Thread: SN74AXC8T245 , SN74AUC244 Hi All,
Please tell me the product with short propagation delay time.
The SN74AVC8T245 has a propagation delay of 1-5nsec. Is there a product with a propagation delay…
Part Number: SN74HC595 Other Parts Discussed in Thread: SN74LV595A , SN74AUC244 , SN74LVC541A Hi good evening,
We tested the SN74HC595N for a VCC of 2V and were not able to get consistent current consumption per the datasheet.
We used a load resistor…
Part Number: LSF0108 Other Parts Discussed in Thread: LSF0102 , SN74AUC244 , SN74AUC1G126 , TXS0108E , TXS0102 Hi Sir,
If Vref_B < Vref_A+0.8V, can be no need to add an pull up resistor? as below schematic.
also, any suggestion for improve when…