Part Number: SN74AUCH16374 Other Parts Discussed in Thread: SN74AUC16374 Hello experts,
What is the difference between SN74AUCH16374 and SN74AUC16374?
For SN74AUC16374 , clock frequency(max) is 275MHz in product folder, but it is difference in datasheet…
Part Number: SN74AUCH16374 Hello team,
My customer asked the any devices which have VLT with the function of SN74AUCH16374.
They want to set the input 1.5V and output 1.8V. Do we have any devices with these feature?
Best Regards,
Austin
Hi,
With the 74AUCH16374DGGR chip, powered with 1.8V, I would like to check that is the best topology to share a single output to 2 FPGA input
Here is the star topology used on existing board:
- 1Q1 pin -> serial resistor -> around 12 inches -> FP…