Part Number: SN74AUP1G04 Tool/software: Hi
The physical screen printing of this product is inconsistent with the specification, please help confirm the reason thank you
Part Number: SN74AUP1G04 Hi Team,
Could you please help check if we have the most updated datasheet to match the device marking of SN74AUP1G04DPWR? If not, please help update the datasheet.
Best Regards,
Jaden Yue
Part Number: SN74AUP1G04 Dears.
As shown below, the SW is located in front of the input pin, so when opened, the level is floating.
Can you lower the output pin to low level by applying a pull-down resistance?
Again, when the SW is short, ask if…
Hi James,
Currently we do not have SPICE model available for SN74AUP1G04. You can search for similar devices which have SPICE model at www.ti.com/spicerack .
Thanks & Regards,
Arpan Gupta
Part Number: SN74AUP1G04 Other Parts Discussed in Thread: SN74LVC1GU04 , , SN74AUP1G14 Hello,
We are using this inverter to achieve signal shaping, both the power rail is 3V, could you pls help review this circuit, and let me know if any suggestion…
Part Number: SN74AUP1G04 Dear Technical Support Team,
I have two questions about SN74AUP1G04.
Could you tell me CI at TA = – 40 ° C to 85 ° C.
Datasheet page.6 shows only 1.5pF at TA = 25 ° C. But the value of CI is blank at TA = – 40 ° C to…
Part Number: SN74AUP1G04SN74AUP1G04DPWR and SN74AUP1G04DF2 specification package is X2SON, but SN74AUP1G04DF2 package is SON, who?
规格书X2SON对应两个不同的封装。之前没注意到。
Part Number: SN74AUP1G04 For part number SN74AUP1G04DSFR, I need the following information: maximum thermal design power, maximum junction temperature (Tjmax) operating and absolute, and the package mechanical drawing.