Part Number: SN74AUP1G04 Hi Team,
I got the following question can you please check:
I’m drawing a footprint for the SN74AUP1G04 Low-Power Single Inverter Gate and I’m not sure whether ‘solder mask opening’ should be really smaller than ‘metal under solder…
Part Number: SN74AUP1G04 Dear Technical Support Team,
I have two questions about SN74AUP1G04.
Could you tell me CI at TA = – 40 ° C to 85 ° C.
Datasheet page.6 shows only 1.5pF at TA = 25 ° C. But the value of CI is blank at TA = – …
Part Number: TMP117 Other Parts Discussed in Thread: LMT70A , SN74AUP1G04 , LMT70 Hi
we are in the process of developing a breakout board for testing our use case probe model, incorporating both LMT70A and TMP117 sensors. Our objective is to achieve an…
Part Number: LMT70A Other Parts Discussed in Thread: LMT70 , TMP117 , SN74AUP1G04 We are in the process of developing a medical-grade thermometer for measuring oral/rectal human body temperature. We plan to incorporate two sensors—one to measure human body…
"Data retention only" means that the device works correctly as long as it does not need to react to any input changing or need to switch any output. When starting up, it is possible that the internal state is not the same as that demanded by the input…
Part Number: SN74AUP1G17 Other Parts Discussed in Thread: SN74AUP2G79 , SN74AUP1G04 , SN74AUP1G74 , SN74AUP1G58 Hello
My customer would like to know dynamic-power data of the below part numbers (ideally 3V VCC and about 2KHz signal).
SN74AUP1G17
SN74A…
Part Number: BQ27426 Other Parts Discussed in Thread: BQ27743 , TCA9543A , SN74AUP1G04 , SN74AUP1G32 , SN74LVC1G3157 Hi there:
I'd like to check those 2 gauge whether have the same I2C address:
BQ27426: 8.3.1.1 I2C interface address: 1010101 BQ27742…
TI has many inverter devices. I would take a look at SN74AUP1G04, SN74AUP1G06, and SN74AUP1G14 for starters. Each are low power, single gate inverters. If you have further questions about inverters I recommend taking that discussion to the Logic forum…