Part Number: SN74AUP1G125 Tool/software: SN74AUP1G125 is a Single 0.8-V to 3.6-V low power buffer with 3-state outputs has no output. ABA experiment shows the buffer IC is bad. I am looking for FAE support to submit IC for RMA?
thanks
Part Number: SN74AUP1G125 Tool/software: Hello,
The SN74AUP1G125 model doesn't seem to have correct behavior when the "/OE" pin is driven HIGH. When /OE is LOW, the input is properly inverted and the output is driven. When /OE is HIGH the input no longer…
Part Number: SN74AUP1G125 Other Parts Discussed in Thread: SN74AUP1G32 , SN74AUP1G97 Dear Sir:
SN74AUP1G125 (Buffer-3 State) output abnormal issue.
1.The input(OE\) of SN74AUP1G125 (Buffer-3 State) is Low.
(1) Rise:
The input(A) of SN74AUP1G125…
Part Number: SN74AUP1G125 Hello Team,
the data sheet specifies a max V_OL of 100mV at I_OL of 20µA and Vcc=0.8V ... 3.6V.
Can you confirm that V_OL,max will be 50mV at Vcc=1.8V?
Will V_OL be reduced to 50mV if I_OL is just 10µA?
Can we expect…
Part Number: SN74AUC1G125 Hello Technocrats ,
The following buffer is used from PHY to iDRAC.
Currently, TI-SN74AUC1G125DCKR is being used as the main source without any issues.
I would like to inquire if TI-SN74AUP1G125DCKR is also suitable for…
Part Number: SN74AUP1G125 Other Parts Discussed in Thread: SN74LVC1G125 , Hi team,
In the datasheet, it says
"The device can produce 24 mA of drive current at 3.3 V, which is ideal for driving multiple outputs and good for high-speed applications…
Part Number: SN74AUP1G125 Dear teams,
My customer is using SN74AUP1G125. They used MCU to give clk signal to the SN74AUP1G125. They found the output has some ringing. Could you help give some suggestions here? Here is the schematic diagram and waveform…
Part Number: SN74AUP1G125 Other Parts Discussed in Thread: SN74LV245A , SN74AHC245 , SN74LXC1T45 Hi
Could you help suggest suitable product s
bidirectional single channel buffer
Vin max: 5.5V IOL: 40mA max.
Part Number: SN74AUP1G125 Other Parts Discussed in Thread: SN74LVC1G17 , SN74LVC2G17 , SN74AVC4T774 Hi team,
My customer has a TDM data stream designed according to the following block diagram, and the following problems need to be solved:
Buffer…
Part Number: SN74AUP1G125 Hi Team,
I am curious about the different between SN74AUP1G125DCKR and 74AUP1G125DCKRG4. According to the DS, 7 4AUP1G125DCKRG4 only has one device marketing, SN74AUP1G125DCKR has several device marketing.
Since, SN7 4AUP1G125DCKR…