Part Number: SN74AUP1G126 Hi team,
Customer is using SN74AUP1G126 in their design. Their circuit as follow.
The output is connected to a voltage divider. OE is controlled by a GPIO, and in this test, it's GND, make this part as highZ mode. The MCU…
Part Number: SN74AUP1G126 Tool/software: SN74AUP1G126DCKR all wire material is Gold which production before 2023 May?
date code 2218 all wire material is Gold ?
Part Number: SN74AUP1G126 Other Parts Discussed in Thread: SN74LVC1G126 The parts are SN74AUP1G126DCKR.
Are there any chances that the following condition will continue to damage the parts?
This is when the 4pin of the output terminal and the power…
Part Number: SN74AUP1G126 Hi Team,
Can you please share your insights about SN74AUP1G126 operating with Vcc of 1.05(+/-0.05)Vcc:
I am actually concerned with the VIL and VIH of this device. With the given Vcc and its tolerance, since the VIL/VIH…
Part Number: SN74AUP1G126 Other Parts Discussed in Thread: SN74LV1T126 Hi team,
I am looking for a 3 state buffer with below specs.
VCC is 2.7V – 3.6V
DCDC_EN is 1.5V
LNA_EN should be above 1.0V
Do we have anything in our portfolio with…
Part Number: SN74AUP1G126 Hi,
The Absolute Maximum Ratings mentions "Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability"
Do you have any documentation that shows if the input voltage is exceeded by x Volt…
Part Number: SN74AUP1G126 Let me ask you a question about SN74AUP1G126.
Is this part a latch-up compatible part?
If it is a compatible part, which description on the data sheet can be used to find out?
Part Number: SN74AUP1G126 Other Parts Discussed in Thread: SN74AUP1G125 I am currently using the pspice models for SN74AUP1G125 and SN74AUP126 downloaded from the TI site. The output Y in my TINA pspice simulation is never in high impedance. state. Is…
Part Number: SN74AUP1G126 Hello, I am using the SN74AUP1G126 in a battery powered device where the OE pin is controlled by a microcontroller but it will be pulled down to keep the buffer disabled by default.
What is the maximum value for the pull down…
Part Number: SN74AUP1G126 Hi,
May i know what will happen to this device when Vcc subject to -0.9V transient voltage undershoot? As per datasheet absolute min is rated at -0.5V. What impact will it have on the device output? Thanks.
Regards,
…