Part Number: SN74AUP1T50 Other Parts Discussed in Thread: SN74AUP1T17 , Hello, Can you, please, indicate the main differences between SN74AUP1T50 and SN74AUP1T17 devices? Thank you, Jose
Part Number: SN74AUP1T17 Other Parts Discussed in Thread: SN74LVC1G17 , TLV3201 , TLV9030 Dear Team,
Please help review following designs and comment. Thanks.
Schmitt Trigger
Input voltage swing is from 3.6V to 1.2V. It could not be recognized by SN74AUP1T17DCKR…
Part Number: SN74AUP1T17 Other Parts Discussed in Thread: SN74LV1T125
Connect 0V to the input pin. Supply 3.3V to the power supply.
When the power supply voltage is between about 0.3V and 0.7V, the same voltage as the power supply voltage appears at the…
Part Number: SN74AUP1T17 Other Parts Discussed in Thread: SN74LV1T34 Hi team,
My customer needs to know the Tj, max & Ψ jt.
I understand Tj is already shown in the below e2e questions.
https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1175723…
Part Number: SN74AUP1T17 Other Parts Discussed in Thread: SN74AUP1T50 What is the difference between these two part numbers? They seem identical.
Thanks
2.2 V is not TTL. And when the input voltage is not near the rails, the supply current indeed increases; see the ΔI CC specification and [FAQ] How does a slow or floating input affect a CMOS device?
Use a level shifter like the SN74AUP1T17.
Part Number: SN74AUP1T17 Hi
I am planning to use SN74AUP1T17 in my design,I simplified the principle of the host side, and we can simply think that the host side can be in two states, floating or driving to low(GND).Because the host can only accept voltage…
Part Number: SN74AUP1T17 Other Parts Discussed in Thread: SN74AVC2T245 , TXB0104 , SN74AXC1T45 hi
please recommend IC to satisfy with below spec.
*change from 3.3V, 1.8V
*need to change 3.3V->1.8 and 1.8V->3.3V
*need buffer type because of UART
please…