Part Number: SN74AUP2G34 Hi,
We are planning to use TI PN SN74AUP2G34YFPR on our Cuircut Board. Can the TI part be underfilled after soldereed onto the board?
Thank you,
Jaz
Part Number: SN74AUP2G34 Other Parts Discussed in Thread: SN74LVC2G34 Tool/software: Hello,
My customer is looking for an IBIS model for SN74AUP2G34D. Is one available? I didn't see it on the TI.com product folder.
Best Regards,
Brian
Part Number: SN74AUP2G34 Hi
My customer has a question. Is it normal for the SN74AUP2G34DCKR output to be slightly lower than the input?
CH1 is input, CH2 is output, the difference between the front and rear is 0.52V
Part Number: SN74AUP2G34 Please tell me the following when a waveform slower than Δt / Δv (Input transition rise or fall rate) is input to the SN74AUP2G34. ・ How does the SN74AUP2G34 work? ・ Is there a possibility that the SN74AUP2G34 will break? ・ If…
Part Number: SN74AUP2G34 Hello,
The TI cross tool lists the SN74AUP2G34DRYR as a p2p replacement for the NC7WV17L6X. That does not look to be the case:
TI part is NOT Schmitt-Trigger input
TI part can only source/sink 4mA. OnSemi part can source…
Part Number: SN74AUP2G34 Hi Expert,
As you can see below, what does ΔICC mean? The current seems too large for a buffer chip. I am just curious. Thanks for help!
BR,
Elec Cheng
Part Number: SN74AUP2G34 Hi Team,
Due to the shortage of SN74LVC2G07DRYR, can we use SN74AUP2G34 to replace it?
I had checked the difference between them, the 2G34 is pull push and 2G07 is open drain output. Is there any issue to place the output…
Part Number: SN74AUP2G34 Other Parts Discussed in Thread: SN74AUP3G34 , , SN74AUC16245 Hi Sir
Reference design use 74AUP2G34 to do 14bit parallel digital video buffer
We will like to check 4bit or 8bit solution ,if have 16bit solution it will be…
Part Number: SN74AUP2G34 Hi Sir
I have a question about SN74AUP2G34 internal architecture.
May I get internal architecture at SN74AUP2G34 as below(like other logic series)?
Since I don't see it in datasheet. Thank you for your great support.