Part Number: SN74AVC16827 Hi Experts
due to thermal simulation requirement .
My customer would like to know the Tc and Tj.
could you provide it
BRs
Brian
Part Number: SN74AVC16827 Hi TI,
My question for you involves the following:
I am using your IBIS model for this part that has DOC and am driving a memory over 2.5" of trace and there is A LOT of overshoot at the load, roughly 2V.
Is the IBIS model…
Part Number: SN74AVC16827 Hi Team,
Could you please give some comments on the output status of SN74AVC16827 when the input is high-impedance?
Thanks.
Best Regards,
Livia Liu
Part Number: SN74AVC16827 Hi Team,
Our customer would like to use only 6 channels of SN74AVC16827 and leave other 4 channels(A6-A10) open, and they'd like to know whether they should put the pullup/pulldown resistor on A6-A10.
Thanks.
Best Regards…
Part Number: SN74AVC16827 It is great the SN74AVC16827 family of logic chips have Dynamic Output Control (DOC) so that no external series damping resistor is required. My questions are:
How long a PCB trace can SN74AVC16827 family of chips support…
Part Number: SN74AVC16827 Hi,
Could you please tell me the interchannel skew(e.g.: between "1A1 to 1Y1" and "1A2 to 1Y2") in the worst case ?
Best regards, Kato
Hi Shreyas-san,
Thank you for your reply.
I found the operating specification on the following website, so I asked you that. Please tell me the maximum output load capacitance when working at VCC = 1.8V and 100MHz frequency if SN74AVC16827 cannot…
Hello,
We would like to use the SN74AVC16827dggr for a camera interface buffer. The clock on the interface runs at 162MHz and it is DDR. The data sheet only specs the propagation delay but not the maximum toggle frequency. Will this buffer run at 162MHz…