Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74AXC8T245 Hi,
This is Venkat from IIT-Madras, India.
We sourced about 25 SN74AVC16T245 ICs for our design over the last one month through Mouser.
We checked a few parts and found that…
Part Number: SN74AVC16T245 Hi Logic Team,
Can you please provide the following information for the TVSOP SN74AVC16T245? I do not see it in the datasheet.
Total power dissipation spec
Best regards, Nic Gough
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74AUC244 Hello
SN74AVC16T245 an support 80MHz clock signal. From B -> To A
VCCA=1.8V
VCCB=2.5V
Thanks
Roi
Part Number: SN74AVC16T245 Hello
I am using the transletor to transle 3.3V digital level from my sensor to the FPGA, could you please check If my connection is ok.
Roi
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: TVP5158 , We need to voltage translate the +3.3V output of the TI TVP5158 Video Decoder to +1.8V to match an FPGA I/O. The 10 bit data is being clocked out of the TI TVP5158 at 108 MHz.
I would…
Part Number: SN74AVC16T245 Hi team,
My customer asks why Vout changes to a high level when Vin is smaller than VIH, and the test waveform is shown below (2B1 represents Vin changing from 1.34V~1.96V, 2A1 represents Vout).
In my opinion, with increased…
Part Number: SN74AVC16T245 Hello Team,
My customer wanted to know the maximum junction temperature ( not ambient, but junction) where the device ( 74AVC16T245DGGRG4) can fully operate? The datasheet shows that the 150C absolute max junction temperature…
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74AVCA164245 , SN74AVCAH164245 , SN74AVCB164245 , SN74AVCBH164245 , SN74AVCH16T245
Hello Team,
My customer is looking for level shifter with requirements below.
- more than 8 channels…
Part Number: SN74AVC16T245-Q1 Could anyone please support in getting pin FMEA for the part no SN74AVC16T245-Q1 for analysis of our Automotive application?
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: DS90LV011A , DS15BR400 , SN74AVC2T245 , SN74LVC8T245 , SN74LVC16T245 , TXU0204 , SN74LXC2T45 Hi,
I am going to tanslate a 200Mbps signal from 1.8V to 3.3V. The SN74AVC16T245 maximum data rate…