Part Number: SN74AVC2T244 Team,
X2SON DQE (1.4x1.0mm) and DQM (1.8x1.2mm) package have slighly different dimension.
Do you know if it is possible to use a PCB footprint that could be compatible for both? The idea would be to enable to solder DQE or DQN…
Part Number: SN74AVC2T244 Hello Experts, I would like to understand VOH and VOL at VCCA=1.8V/VCCB=3.3V condition. According to datasheet, VOH and VOL vary by output current and power supply voltage. How can I understand VOH/VOL? VOH(min)=VCCB-2V, VOL(max…
Can SN74AVC2T244 also act as a suitable substitute ? Can you help me with the internal working of SN74AVC2T244, maybe an ideal working circuit too ? Didn't find much in the datasheet for this.
Part Number: SN74AVC2T244 In the datasheet, I see that sn74avc2t244dqer and sn74avc2t244dqmr have the same package x2son, but they are not consistent in the size drawing. Please help to determine whether the dimension drawing is correct? If it is correct…
Part Number: SN74AVC2T244 Hi, support team
Could you find the alternative parts for SN74AVC2T244DQMR? (need 1000 nos)
Thanks so much, Best regards, Yuki
Part Number: SN74AVC2T244 The question has come up as to where the SN74AVC2T244 can handle a 3.3V input signal when its VCC is 1.8V. It appears to me that the datasheet implies that it can by saying the absolute max input is 4.6V and does not related…
Part Number: SN74AVC2T244 Other Parts Discussed in Thread: SN74AUC244 Hello,
We are planning to use the SN74AVC2T244 as a converter from either 3.3V or 1.8V to 1.35V. The part is expected to drive 8 loads (2 mA per load).
According to the datasheet…
Part Number: SN74AVC2T244 Hello TI,
Should the I_OH Test Conditions in sces767b in row V_OL not perhaps be I_OL and V_I = V_IL (V_H does not seem to have been defined anywhere)?
Part Number: SN74AVC2T244 Hi,
The output drive current is +/- 24mA on page 1 of SN74AVC2T244 data sheet. So, is this value the current for each output channel? Or, is this value the total output current?
Best regards, Kato