Part Number: SN74AVC2T244 Dears
We have one use case of SN74AVC2T244, VCCA = 3.3V, VCCB =0V, direction from A to B, and OE = 1, in this condition, how about the supply current and leakage current, thanks.
Jun Shen
Part Number: SN74AVC2T244 Hello,
Can you please clarify for me what the output high, min and output low, max voltages are for the SN74AVC2T244, if VCCA = 1.8V and VCCB = 3.3V. The electrical characteristics on data sheet seems ambiguous and reads as if…
Part Number: CC2674R10 Other Parts Discussed in Thread: SN74AVC2T244 Tool/software: I'm working with a customer who is using the SN74AVC2T244 as a level translator between another MCU and the CC2674 device. We are finding that the drive strength of the…
Part Number: SN74AVC2T244 Other Parts Discussed in Thread: SN65MLVD203 , 2N7001T , , SN74AXC2T45 SN74AVC2T244Dear Sirs
I'm interfacing a 1.8v output FPGA to a 3.3V MLVDS system that will be running at 100MHz. I plan to have the 1.8V FPGA output feed…
Part Number: SN74AVC2T244 Hi Team, I would like to ask for your support for the customer inquiry below regarding /OE pin of SN74AVC2T244 Base on the datasheet, The SN74AVC2T244 is designed so that the OE input circuit is referenced to VCCA. Our customer would…
Part Number: SN74AVC2T244 Hello TI,
Please provide us values of following parameters for SN74AVC2T244DQER:
Maximum Thermal resistance (junction to ambient)
Maximum Junction Temperature
Regards,
Purvi
Part Number: SN74AVC2T244 Hi I have selected SN74AVC2T244DQER Part for level translator.
To get output with respect to input, 4 pin(/OE) should be connect to ground or connect to VCC.
Part Number: SN74AVC2T244 Other Parts Discussed in Thread: SN74AVC4T245 Hi,
May I know is there any other IC from TI which is equivalent to SN74AVC2T244.
I need an IC with same functionality but some simple package like TSOP.
Note:Output enable is a must…