Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74LVC2G34
I am using SN74AVC2T45 level translator for driving a bicolour led. Since DIR pin is grounded, data flow is B to A. If the circuit to work, SN74AVC2T45 should be capable of sinking…
Part Number: TXV0106-Q1 Other Parts Discussed in Thread: SN74AVC2T45-Q1 , Please provide IBIS model and project details as follows
Device name of the model you are requesting :
SN74AVC2T45-Q1
TXV0106-Q1
Project details :
For simulating a…
Part Number: SN74AVC2T45-Q1 Because datasheet mentioned that this part is "Qualified for Automotive Applications".
Is it qualified for AEC-Q100 or AEC-Q200?
Thanks.
Part Number: SN74AVC2T45-Q1 Other Parts Discussed in Thread: SN74AVC2T45 Hi Team,
I am looking for an AEC-Q part with low tpd.
The application is to make two copies of the same signal (They don't have to be zero delay outputs). tpd is more critical…
Part Number: SN74AVC2T45 Hello,
Can you please help to explain why these components would be marked with "TD7" instead of "TDN" as it calls out on the datasheet and on ti.com. We have a customer who is questioning the marking so I would like to provide…
Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74AXC2T45 Hi All,
I have a question about SN74AVC2T45.
As shown in the data sheet below, there is a delay time, but is there a difference in the timing when B1 and B2 are output? I want to…
Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74AXC2T45 Hello, My customer would like to use SN74AVC2T45 as 1.8V to 3.3V level shifter for a 50% duty cycle clock, not data stream Datasheet says max data rate for 1.8V to 3.3V is 500Mbps,…
Part Number: SN74AVC2T45 Hi Team,
Our customer would like to confirm if the devices below are multi-component semiconductor (MCO). I have confirmed that these devices are single die but are they MCO?
SN74AVC2T45YZPR SN74LVC1G08DRL SN74LVC1G17DBVR…
Part Number: SN74AVC2T45 Other Parts Discussed in Thread: SN74AUP1T34 , SN74AXC1T45
Hi guys,
I want to know if you can help me to understand if this IC can tolerate and handle the input pins(B) has a different logic level than the voltage supplied…
Part Number: SN74AVC2T45 Hello, i wanted to ask if there is any Level-Shifter with Enable-Pin as well as with DIR-PIN? On the Datasheet is written that the VREF-A and B should have a value between 1.2 V to 3.6 V. My second Question is: how could I disable…