Part Number: SN74AVC4T774 Hi, I am using the SN74AVC4T774 bus transceiver and have a question around propagation delay. Has the part-to-part skew been characterised for this IC and if so, does it differ from the min to max propagation delay highlighted…
Part Number: SN74AVC4T774 Hi team,
Is it acceptable to use the SN74AVC4T774 with the following supply voltages on the A-side and B-side?
VCCA = +3.3V
VCCB = +1.8V
In the "Typical Application Circuit" shown on page 2 of the datasheet, VCCA…
Part Number: SN74AVC4T774 Hi,
Should the thermal pad of SN74AVC4T774 be connected to GND or left floating? I couldn't find this information in the datasheet.
Thanks,
Jamal
Part Number: SN74AVC4T774 The SN74AVC4T774RSVR level translator is configured with VCCA = 3.3 V and VCCB = 1.8 V . During power‑up, the 1.8 V (VCCB) rail is measured at approximately 2.2 V instead of 1.8 V. If I connect VCCA=1.8V,VCCB=3.3V it works properly…
Part Number: SN74AVC4T774 Hi Team,
We have recived the folllowing PCN for the below part : SN74AVC4T774PWR
Could you please confirm is this PCN will impact on Fit, form and function.
PCN20260409005.1A.pdf
Thanks,
Nitin Gond.
Part Number: SN74AVC4T774 Hi,
I would like to confirm the function of the buffer symbols (triangle marks) shown in the logic diagram of the SN74AVC4T774.
Is it correct that these internal buffers digitally receive the input signal and regenerate a…
Part Number: SN74AVC4T774 Tool/software: Dear TI E2E,
I am using the Bus Transceiver with VCCA=1.8V, what is the max. recommended voltage at OE_L?
Thank you.
Milorad.
Part Number: SN74AVC4T774 Sehr geehrtes Team von TI,
pcn-attachment-1.pdf
ich habe folgende PCN von Ihnen bekommen.
Wo kann ich die Samples bekommen um das BAuteil zu prüfen?
Wir verwenden folgendes Bauteil: SN74AVC4T774RGYR
Vielen Dank schon…
Part Number: SN74AVC4T774 Hello,
I would like to request a Letter of Volatility (LOV) for part number SN74AVC4T774 to find out if this part contains volatility or non-volatility memory. I believe part number SN74AVC4T774 is the same part as 74AVC4T774RSVR…