Part Number: SN74AVC4T774 Hi team,
I'm Ives Li, FAE in SZ AA1 team.
My customer TCL is using SN74AVC4T774 in their application as showed below:
And they found that the MISO input from SPI1 cannot be pulled down by SoC and SPI2, it will affect the…
Part Number: SN74AVC4T774 Other Parts Discussed in Thread: SN74AXC4T774 Hi Team
Can you specify what is the power consumption of the SN74AVC4T774 from each power rail according the following conditions
1. 10MHz 4wire SPI interface
2. VCCA - 1.8V
3. VCCB…
Part Number: SN74AVC4T774 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
I'm looking for the time needed for the dir change to be effective. (turnaround timing ?). Just to be sure my request is clear, If the component is A …
Part Number: SN74AVC4T774 Hi
I am not using 2 I/O pins of this level translator. What to do with DIR3 and and DIR4 - need to float or connect to GND?
if I connect it with GND with 100K PD then on port B(B3 and B4) side do we need to provide PU/PD or…
Part Number: SN74AVC4T774 Other Parts Discussed in Thread: TXU0304 , TXS0206 Hi Team,
A customer is looking to replace Nexperia 74AVC4TD245 in their schematic. I suggest using SN74AVC4T774 as an equivalent, however, due to the limited layout space, they…
Part Number: SN74AVC4T774 Hi,
We are using the SN74AVC4T774RGY in our new design. This part is a VQFN (16) package. Can anyone confirm whether the centre pad of this pad must be connected to the ground or if it can be kept as floating?
Thanks,
Jab
Part Number: SN74AVC4T774SN74AVC4T774 is adopted, but it is used as HDMI output.
Please tell me how to find the output impedance when outputting from the B port.
Wiring resistance is 50Ω.
Part Number: SN74AVC4T774 Other Parts Discussed in Thread: SN74AXC4T774 , SN74AXC2T45 Hi
SN74AVC4T774RSVR any suggested alternative materials? Mainly to reduce the size
Part Number: SN74AVC4T774 Hi Ti team
If i connect PIN#5, 6 to GND and pin#9, 10 GND, do we need to connect pin 3 and 4 to GND or can we leave it float?
Part Number: SN74AVC4T774 Hi,
The level translator IC SN74AVC4T774PWR is being used in one of our projects for 1.8V-3.3V translation or vice versa. One of the outputs (B4) is being removed as part of the latest revision of our PCB. In the datasheet, it…