Part Number: SN74AVC8T245-Q1 To whom it may concern -
In the datasheet, it states that "To ensure the high-impedance state of the outputs during power up or power down, the OE input pin must be tied to VCCA through a pullup resistor and must not be…
Part Number: SN74AVC8T245 Hello forum,
new to the whole simulation task and still learning a lot everyday.
I was simulating a track in the multiboard project I was tasked to analyze and I mistakenly did not configure correctly the input of the level shifter…
Part Number: SN74AVC8T245 Other Parts Discussed in Thread: SN74AXC8T245 Hi Team
Customer plans to find level shift device used for RGMII. they are interested in these two devices: SN74AVC8T245 and SN74AXC8T245
Can you show the difference between these…
Part Number: SN74AVC8T245 Hi Team,
If we only power VCCA or VCCB, will it have leakage current at the power down side? If it has, what's the approximate number?
Does the Ioff means the current at the power down side?
If there is any problem even if…
Part Number: SN74AVC8T245 Hi team,
One thing want to check, what is the state of the output pin when there is no signal at input? High level, low level or high impedance?
BR
Adrian
Part Number: SN74AVC8T245 Other Parts Discussed in Thread: SN74AXC8T245 Hi team.
can the SN74AVC8T245 be used for the RMII application?
and how is the drive ablilty for that?
Part Number: SN74AVC8T245-Q1 Other Parts Discussed in Thread: TXU0104-Q1 Hello, I am looking at the datasheet for SN74AVC8T2450-Q1 page 17:
There is a pull-up on the DIR pin, how do I calculate the value of the pull-up resistor?
Thank you,
Joe
Part Number: SN74AVC8T245 Hi, Expert
my customer want to use SN74AVC8T245 from 1.2V to 3.3V. but in the datasheet, 1.4V to 3.6V is optimized Vcc range.
could you help to clarify what is the difference between 1.2V to 1.4V and 1.4V to 3.6V? thanks.
BR …
Part Number: SN74AVC8T245-Q1 Hi Experts,
In datasheet page 3, 'Pin Functions' Table DIR pin (pin 2) for a TSSOP package doesn't exist. Is the datasheet correct? Please confirm. If not, we will submit documentation feedback to correct this if needed.…
Part Number: SN74AVC8T245 Hi,
We are using SN74AVC8T245RHLR in a design.
Due to current availability and long lead time issues, We are checking if we could find any alternate parts instead of SN74AVC8T245RHLR.
We came across CAVC8T245QRHLRQ1 which seems…