Part Number: SN74AXC2T245-Q1 Hi Team,
We accidentally made an error during schematic drafting.
The direction pins were connected to VCCB instead of VCCA . However, the circuit is currently functioning properly, and we have not observed any issues…
Part Number: SN74AXC2T245-Q1 Hi,
Our HW team is looking for Board Level Reliability Temp Cycling Test report for part below to perform solder joint robustness simulation. Please support.
SN74AXC2T245-Q1
Part Number: SN74AXC2T245-Q1 Hi TI team,
We are using SN74AXC2T245RSWR part in our design as a buffer(3.3V to 3.3V). Could you please tell us the maximum data rate achieved per lane in this application.
Warm Regards,
Mythili B
Part Number: SN74AXC2T245 Tool/software: Hi Support Team,
In the SN74AXC2T245RSWR datasheet, I could only find the MAX and MIN values for the switching time. Would it be possible to provide the TYP value?
Thank you!
Part Number: SN74AXC2T245 Tool/software: There are 2 dots on part marking for the 'RSWR package. What is the significance of these extra laser dots on the Top Marking? This is not called out on the D/S and is not signified in our internal PN part marking…
Part Number: SN74AXC2T245 Tool/software: Dear
We use SN74AXC2T245 to translate CS SPI signal from 1,8 V rail to 3,3 v Slave device, according to data sheet there are internal pulldown of 74 ko inside IC on I/O lines so in case of Pullup is needed…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74AXC2T245 , , TXV0108 , SN74AVC8T245 , TXV0106 Tool/software: Hi TI Team,
I am planning to use SN74AXC8T245 / SN74AXC2T245 to level shift from 1V2 to 1V8 for 1000Mbps GMII interface in my…
Part Number: SN74AXC2T245 Tool/software: Hello team,
When the connection to the IC is shown below figure, are B1 and B2 in HiZ status?
Best regards,
Shotaro