Part Number: SN74AXC4T774 What is the guaranteed maximum time from a DIR pin transition to valid output data on the SN74AXC4T774, with OE held low? We need this to validate a 2-wire JTAG turnaround budget at VCCA=1.2V, VCCB=1.2-1.8V.
Part Number: SN74AXC4T774 Other Parts Discussed in Thread: TXV0108 , TXV0106 For SPI timing analysis, can TI provide the maximum channel-to-channel skew between a translated clock channel and a translated data channel in the SN74AXC4T774?
Part Number: SN74AXC4T774 Hi,
I would like to know whether I can tie / OE signal of SN74AXC4T774 to GND directly ?
I saw the datasheet mentioned that SN74AXC4T774 has 71K ohm integrated weak pull-downs on all data I / Os .
It seems to me that it…
Part Number: SN74AXC4T774 Other Parts Discussed in Thread: SN74AVC4T774 , Hi ti team,
Is the software compatible between SN74AXC4T774 and SN74AVC4T774?Thanks!
Part Number: SN74AXC4T774 Hi AE,
1. Can the SN74AXC4T774 be used as an SPI buffer?
2. If the SPI speed is 63 MHz, can this device support it?
Best Regards
Part Number: SN74AXC4T774 Hi AE,
1. Can the SN74AXC4T774 be used as an SPI buffer?
2. If the SPI speed is 63 MHz, can this device support it?
Best Regards
Part Number: SN74AXC4T774 Hi AE,
1. Can the SN74AXC4T774 be used as an SPI buffer?
2. If the SPI speed is 63 MHz, can this device support it?
Best Regards
Part Number: SN74AXC4T774 Tool/software: Hi
If input signal slew rate is 5V/ns then what will be output slew rate when translating down as below with 100 MHz frequency.
Case1: 3.3V to 0.8V (A to B)
Case2: 3.3V to 2.5V (A to B)
Will it keep maintain…