Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74AXC4T774 Hello,
I'm looking at the SN74AXC8T245 and SN74AXC4T774. Where in the datasheet can I find the drive current capacity for each output pin? I took a quick look, but was having trouble…
Part Number: SN74AXC8T245
I saw in the datasheet of SN74AXC8T245 that,“Simultaneous up and down translation is supported when both VCCA and VCCB are at least 1.40V.”.
I don't quite understand the specific meaning of " Simultaneous…
Part Number: SN74GTL2014 Hi,
I used GTL2014 and AXC8T845 from both direction level translator on adaptor board.
IO from silicon to port B of GTL2014 (vref 0.5V) with 71.5ohm PU resistor to 0.91V , port A (3.3V) of GTL2014 direct connect to port A (1.2V…
Part Number: SN74AXC8T245 1、Whether the I/O ports at both ends of the chip can be added with pull-up resistors or pull-down resistors?(just like below figure);Some IO ports need to be given a high/low level voltage initial state.
2、Could you show me…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74LVC1G07 , LMV7219 Hi
Does TI have 1.8V to 0.5V level shift? Data rate need abobe 20Mhz.
We use 74AXC8T245 but it only support to minimum 0.65V.
Thanks!
Jeff
Part Number: SN74AXC8T245 Looking for a RAD hard part candidate to use as a level shifter between a 3.3V uP and a 5V output data. To be used in military or space environment, Similar to p/n SN74AXC8T245.
Part Number: SN74AXC8T245-Q1 Hi Expert,
My customer is using SN74AXC8T245QPWRQ1 in their project. When they do the Propagation Delay timing test , VCCA=1.8V , VCCB=3.3V ,the delay between B6 → A6 ( UART_TX )is more than 4n.
In actual the sourcing and end …
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74AXC4T245 , SN74AXC2T245 , SN74AXC4T774 Hi myTI support I want SN74AXC8T245's PSpice model. Or SN74AXC4T245 or SN74AXC2T245 is fine. Thanks, Ueyama