Part Number: SN74AXC8T245 Hello TI Experts,
In my application, SN74AXC8T245 is planned to be configured into the mode highlighted below. VCCA is connected to 1.8V and VCCB to 3.3V. My proposal is that the OE is tied to GND directly, both DIR1 and DIR2 are…
Part Number: SN74AXC8T245 I am trying to simulate a design that translates from 1.8V to 2.5V using the SN74AXC8T245 part. There is no model variant in the IBIS file for 2.5V - do you have a recommendation for how to proceed?
There are two parts in my…
Part Number: SN74AXC8T245 Hello, Found this device from a TI application report. The data rate supported is 380mbps for 1.8V translation as per datasheet. May I know what is the translation rate for 1.2V VCCA? Hope anyone reply soon
Thanks
Part Number: SN74AXC8T245 Hi Team,
Our customer would like to know if the SN74AXC8T245 voltage translator can drive a 50MHz clock with a data line synchronously?
Regards,
Danilo
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: TXU0104-Q1 Hello, I am looking on page 23 of the datasheet for SN74AXC8T245-Q1:
I would like to know how the value of the pull-up resistor on DIR1 is determined?
Last, is it necessary to add…
Part Number: SN74AXC8T245 Hello,
I am looking at the SN74AXC8T245 to be used for SDIO2.0, which uses a clock frequency of 50MHz.
Please confirm if this device can be used for SDIO2.0. Any help is appreciated.
Thanks and best regards,
Seong
Part Number: SN74AXC8T245
If the device is completely powered down (both Vcca and Vccb at 0V) is it acceptable to drive the IOs (i.e. have voltages present on signals connected to the IO pins)? Based on the abs max ratings I’d say yes but the description…
Part Number: SN74AXC8T245-Q1 Hi,
I'm looking at the SN74AXC8T245-Q1 datasheet Table 8-1 functional table. I wanted to confirm that if this table is correct? I wanted to verify the accuracy of bits 5:8 direction base on DIR2. I've added a screenshot,…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74AVC16T245 , SN74AVC8T245 We are using a 1.5V MAC that needs to be connected to a 3V3 PHY via a RGMII bus. We are planning to have a 1000Mbit/s connection via this RGMII interface.
We want to…