Part Number: SN74AXCH8T245 Tool/software: Hello,
Can I connect several outputs of SN74AXCH8T245 together if I also connect the corresponding inputs together? I am hoping to get more drive strength than 12mA. I cannot use the equivalent LXCH device…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 I designed a circuit using the Telit GE190C1-EUX GSM modem. Since the GSM side operates at a 1V8 voltage level and my processor operates at a 3V3 level, I used the SN74AXCH8T245…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: TXV0108 , TXV0106 Tool/software: We are currently using your level shifter PN SN74AXCH8T245PWR wired similar to what is shown in your app note Scea065B, Section 2.5.1 with level shifters from…
Part Number: SN74AXCH8T245 Tool/software: Hi,
Could you correct package size of SN74AXCH8T245 PW on first page in datasheet?
Other datasheet, package size include lead length but SN74AXCH8T245 PW package exclude lead length.
So customer is confusing…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74LVC2T45 Tool/software: Dear team,
We are using SN74AXCH8T245RHLR in our design,We need to know the maximum IO toggling speed of the mentioned chip.Kindly support.
Thanks & Regards, Blessing…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74LVC1G3157 , TS5A63157 , SN74LVC2G53 Hi,
We are using SN74AXCH8T245PWR in our design to convert 25MHz signal from 3.3V to 0.75V. When we got the board and test it, we see that this part…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: TXV0106-Q1 , SN74AUC34 , TXV0108-Q1 Hi,
Does SN74AXCH8T245 suitable for below application?
We need to use it for the signals on Ethernet MAC GMII. 1.5V to 1.8V (1.8V to 1.5V). The signals…
Part Number: SN74AXCH8T245 I am looking for the level translator between 3.3V and 1.2V (uni or bi-direction) at >200Mbps. Does SN74AXCH8T245 meet this requirement? (cannot see speed rate at 1.2V from the datasheet). If not can you recommend one?
Thanks…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 , , SN74AVCH8T245 Dear Sir:
The current system uses SN74AXC8T245 as the I2S&SPDIF buffer.
Because SN74AXC8T245 is out of stock recently, can I use SN74AXCH8T245 instead?
…
Part Number: SN74AXCH8T245 I need to translate a 1.8V, 5ns pulse to 3.3V. Will the SN74AXCH8T245 work? If not does TI have a better solution?
Thanks,
Kevin