Part Number: SN74CB3T3257 Other Parts Discussed in Thread: TMUX1574 , , SN74CBTLV3257 Hi Team,
My customer wants use this part for SPI signal transmission and they want to know this device output length limit.
from my understanding we can calculate…
Part Number: SN74CB3T3257 E2E,
I'm looking for a mux that can also act as level translator. A 2:1 high speed 4-channel mux, with each channel capable of working at different voltages.
Typical application:
One Jtag connector with many chips on…
Part Number: SN74CB3T3257 Is SN74CB3T3257PWR a fully bi-directional switch?
Is the switch electrical behavior identical on both directions, A ports to B ports and B ports to A ports?
I am asking this because I performed the following test:
I placed…
Part Number: SN74CB3T3257 Other Parts Discussed in Thread: TS3A24157 , SN74AVC1T45 Hi,
We are using SN74CB3T3257PWR device. This is powered by 3.3V but the IOs we are providing is at 1.8V logic. Please share confirmation that this device supports 1…
Part Number: SN74CB3T3257 Other Parts Discussed in Thread: TS3A5018 , CD40109B I would like to find a 4-BIT 1-OF-2 FET MULT/DEMUL, like as SN74CB3T3257, to support output voltage translation tracks VCC and the VCC can up to 5.5V or more. Customer hop…
Hi there,
The datasheet specifies the Ron value for 2.3V VCC and 3V VCC with the Vi set to 0V. It doesn't show what the Ron would be with Vi at various values such as 1.7V or 2.4V. Unlike the CB3Q which have a pretty flat Ron response, the CB3T is likely…
Part Number: SN74CB3Q3257 Other Parts Discussed in Thread: SN74CB3T3257 Tool/software: Hi Expert,
Is there any part available in TI which has both Mux/demux and level shifter functions in one IC. It may be 4-bit, 8bit or 16 bit.
Regards,
Kaviya…
Part Number: TMUX136 Other Parts Discussed in Thread: TMUX154E , , SN74CB3T3257 Hi Expert,
Customer would like to check does TI has solution for I3C HUB /I3C MUX / I3C level shift?
And could it support I3C high voltage(3.3V)?
Regards,
Mark
Part Number: TS3A27518E-Q1 Other Parts Discussed in Thread: TS3A27518E , SN74CB3T3257 Hi Team,
Whether TS3A27518E-Q1 could achieve logic and also achieve level shift at the same time?