Hey Ashwini, Looks like you rejected this answer. Did you have any extra questions or thoughts here? Can you maybe share what your inputs and outputs are and what you're using to simulate to help with our debugging and check is what you're seeing is expected…
Part Number: SN74CBT3125 Other Parts Discussed in Thread: TMUX1111 , SN74LV4066A Hello guys,
One of my customers is considering using SN74CBT3125 for their new products.
At this moment, they have the following question.
Could you please give me your reply…
Part Number: SN74CBTLV3125 Other Parts Discussed in Thread: SN74CBT3125 , Hello expert,
Customer is facing supply issue on SN74CBTLV3125DBQR. We would like to know if SN74CBT3125 could replace SN74CBTLV3125. It seems like VCC is a spec we need to discuss…
Hi Paul,
I am closing this thread as I have not heard back from you in some time - if you have any other questions please start a new thread and one of our applications engineers will respond to you.
Best,
Parker Dodson
Part Number: SN74CBT3125 Does this chip handle i/p with 1.8V logic? (Please note, VCC is 5V and OE pins are Tied to Gnd)
When 1.8V applied on any of the I/P, Same can be seen on O/P?
Will there be any drop?
Can i configure 1.8V on 2 Switches and 2 Switches…
Part Number: SN74CBT3125 Can we connect the VCC pin of this SN74CBT3125 switch chip to an I/O pin of a 430 MCU? In other words, can we use the I/O pin output of a 430 MCU to supply the power to the switch chip? What we want to do is to control the power…
Part Number: SN74CBT3125 Hi sir,
I have two question need confirm about SN74CBT3125 as bellows:
(1) When SN74CBT3125 OE# signal assert, the Pin A and Pin B status. Does the pin A and Pin B is unstable status or tri-state?
(2) When SN74CBT3125 OE# signal…
Hi Bryan,
The SPI clock rate support 20M/33M/50MHz.
Customer is not really sure about Intel definition on CIN (marked FET component criteria).
SN74CBT3125 is used on Intel reference design so I would assume it meet intel requirement and we only need a…