Part Number: SN74CBT3257C
Hello,
One of my customers have used the Fairchild IC - FST3257 in their projects and recently they decided to replace it to a direct replacement from TI - the SN74CBT3257C. They have 3 ICs of the FST3257 in their board and…
Part Number: SN74CBT3257C Other Parts Discussed in Thread: TMUX1574 Team,
The datasheet absolute maximum ratings show Continuous current through VCC or GND terminals at +-100mA.
My customer's 5V supply is only rated for 50mA. It is unclear what could…
Part Number: SN74CBT3257C Other Parts Discussed in Thread: SN74CBT3257 Hi team,
Is it possible to provide the thermal data (i.e. Tj, θja, θjc, Pd) of SN74CBT3257CRGYR?
Best Regards,
Leroy Song
Part Number: SN74CBT3257C Thank you for your help.
I would like to ask you a question about your device N74CBT3257C.
I am planning to use this part in an audio switching circuit.
Use with power supply voltage 5V
doing.
For the input signal, a diode…
Part Number: SN74CBT16214C Other Parts Discussed in Thread: SN74CBT16292 , SN74CBT3257C Hi,
There is any other part with 8 or 12 bit channel for 1:2 mux
specifications should be similar to 1:3 MUX 12 bit SN74CBT16214C.
Part Number: TS5N412 Other Parts Discussed in Thread: SN74CBT3257C Tool/software: This is for a part that is being discontinued. We are currently using an Onsemi (74FST3257DTR2) and, datasheet wise, it looks like a good change to TI (TS5N412PW).
During…
Part Number: TMUX1575 Other Parts Discussed in Thread: SN74CBT3245A , SN74CBT3245C , SN74CBT3861 , SN74CBTLV3861 , SN74CBT3257C , TMUX1574 , , SN74LV4066A , TMUX1511 , TS5A23157 , TMUX1072
System isolation is critical for power sequencing, managing…
Hi, you are welcome!
check out this thread: CB3Q3257 Ron . The images are quite small but you can see, that Ron stays below the Ron,max from the datasheet.
We recommend to apply VDD first, OE and S don't matter.
The SN74CBT3257C should run with…