Part Number: SN74CBTD3384 Hi Team,
Currently using ZNYQ FPGA, there is a problem of IO being injected with current by external devices.
Can SN74CBTD3384 solve this problem?
Part Number: SN74CBTD3384 Other Parts Discussed in Thread: ADC121S101 , Hi expert,
Customer connects 1 CH (pin10) of SN74CBTD3384 with 3 nCS pins of 3pcs of ADC(ADC121S101) together. Sometimes this channel fails (pin10 shorten to pin20, that is shorten to…
Part Number: SN74CBTD3384 Other Parts Discussed in Thread: TMUX646 Hi team,
Do we have a newer device to update the SN74CBTD3384, which is a 10 bit switches with level shifter? Thanks.
Part Number: SN74CBTD3384 Hi.
Just one little question :
Which port of the SN74CBTD3384 is the source? A or B?
I wonder which port I should connect 3.3V signals or 5V signals.
Can I connect 3.3V signals to any port?
Thanks.
Part Number: SN74CBTD3384
There are many methods where one would like to tie multiple sets of digital blocks (DSPs, FPGAs, MCUs, CPUs, etc) at a specific voltage(5V) to just one FPGA but of a lower voltage (3V3). One of the methods is using a SN74CBTD3384…
Other Parts Discussed in Thread: SN74CBTD3384 I am planning on using the SN74CBTD3384 in my design to interface 5Vdc input commands to a 3.3Vdc CPLD. There are a few questions I have that I cannot figure out a solid answer from the data sheet. 1) When…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: DRV135 , , LSF0108 , SN65HVD82 , SN74CBTD3384 Hi Everyone,
I use SN74LVC16T245DGGR to translate voltage level between MCU (3.3V) and RS485 transceiver (5V). Aditional, MCU generates audio tone then…
Hi
Thanks for your response.According to your suggestion,i have a new design for TMS320F2812 power.As you see,because i use SN74CBTD3384 to transform between 3V3 and 5V ,SN74CBTD3384 needs power between 4.5V to 5.5V,so i need to monitor VIN,when VIN lower…
Hi Leo,
Please see details below for your query on SN74CBTD3384C:
1. When the switch is on, it means both sides of bus switch (A and B) each has a 6.25pF (Total 12.5pF I/O capacitance between A and B)
2. What maximum operating frequency are you looking…
Part Number: SN74CBTD3861 Other Parts Discussed in Thread: SN74CBTD3384
Dear E2E Community,
One of my customer use the SN74CBTD3861 devices for down translation between DSP (5V) and FPGA (3.3V) and it works properly.
However, when there is no FPGA program…