Part Number: SN74CBTLV3245A Kindly share the Top Side Marking Format or Guideline for row #1 of MPN : SN74CBTLV3245ADBQR. Seems TI removed this information from the website.
Row #1 Marking :
11A6E1K G4
Thanks.
PT
Part Number: SN74CBTLV3245A Hi team,
Nice to meet you by email. Currently, my customer has a new Router project with SN74CBTLV3245A. OE of SN74CBTLV3245A is controlled by CPLD. When testing, they found “stepped voltages” at OE pin as below. please help…
Part Number: SN74CBTLV3245A Hi Team,
Our D/S requires the control pin of SN74CBTLV3245A should not be float, which should be connected w/ Vcc or GND. Does this requirement also applies to I/O pins of this device? Or customer can leave I/O pins float when…
Part Number: SN74CBTLV3245A
Hi team,
My customer is using the SN74CBTLV3245A now. As the datasheet we need to pull up/low the unused pins. Currently we set the A7pin float(unused), B7 pin to GND, whether it has risks? Thanks.
Part Number: SN74CBTLV3245A Other Parts Discussed in Thread: TMUX1511 Hi,
We have finalized SN74CBTLV3245APWR for using it as switch between Ultrascale Plus FPGA and SPI bootflash.
SPI bootflash supports max clock frequency of 166MHz.
But, we are using…
Part Number: SN74CBTLV3245A Hello,
I am using SN74CBTLV3245ARGYR in Hillside RCB. It has a center pad and there is not much description about it. I would like to check if it needs to be connected to GND or just soldering to the PCB is good enough?
Solution…
Part Number: SN74CBTLV3245A
I need to analyze Signal Integrity of a 20Mhz clock net. In the middle of nets we use switch. I downloaded IBIS model sn74cbtlv3245a.ibs from TI. I have a questions about how to use this ibis model on ADS platform.
(1)I import…
Part Number: SN74CBTLV3245A Hi team,
My customer is using the SN74CBTLV3245 now. We want to check whether the logic input has slew rate requirement? Thanks.
Part Number: SN74CBTLV3245A Although the MAX value of VIH and the MIN value of VIL are not described in the table of Recommended Operating Conditions in the data sheet, can you consider it as an acceptable value up to the rated value?
( MAX of VIH : 4…
Part Number: SN74CBTLV3245A I noticed that the tpd is *higher* at a higher VCC. This does not make sense to me. Why would the tpd be higher with a higher VCC voltage? Shouldn't it be lower?