Alberto, The closet p2p device in a 16 pin SOIC package I found that will support voltages from 0 to Vcc is the SN74CBTLV3251. This device supply voltage goes up to 3.6 V. Thank you, Adam
Part Number: SN74CBT3251 Other Parts Discussed in Thread: MUX506 , SN74CBTLV3251 , SN74CB3Q3251 , TMUX1208 Dear sir,
There is a problem when I use multiplexer SN74CBT3251. The signal source is an 50 MHz optical receiver which convert the optical on/off to…
Hello Gabe,
If SPI master's driving strength is capable of handling 60 SPI slaves, what you need is to multiplex CS0~CS7. Using 8 unit of SN74CBTLV3251 or SN74LV4051A, 1:8 de-multiplexer, or 4 unit of CD4097B, 2-channel, 1:8 de-multiplexer, should be…
Other Parts Discussed in Thread: SN74CBTLV3251 , SN74CB3T3257 , TS3A44159 , CD4512B Hello!
I need a few signal switches, but I cannot figure out whether to use digital multiplexers or analog switches.
I need a couple of quad 2:1 muxes, a couple of single…
Other Parts Discussed in Thread: CD4067B , TS3A44159 , TS3A27518E , SN74LV4051A , SN74CBTLV3251 , CD74HC4067 Could you recommend analog MUX with 1.8V operation?
12 inputs go into 1 output. one chip solution is ideal. Discrete solution is acceptable.
You could also consider SN74CBTLV3251 which is 1:8 Mux operates at 3.3V and has ioff feature which will prevent unwanted conditions during power down conditions. Please let know what you go with.
Part Number: TCAN1042GV-Q1 Other Parts Discussed in Thread: SN74CB3Q3251 , SN74CBT3251 , SN74CBTLV3251 , TCAN332
Any design examples/circuits for muxing CANH/CANL onto various pins? I have a need to be able to drive these connections into various pins on…
Other Parts Discussed in Thread: CD4051B , SN74CB3Q3251 , SN74CBTLV3251 Team,
What is state of the I/O channels when the CD4051B is configured as a demultiplexer at the beginning of power-up (rising edge of voltage supply)?
Pins A,B,C are shorten to ground…
Hi Carlo,
I found the following e2e posts on ESD information for these parts:
Note we have a new pin-to-pin replacement for SN74CBTLV3125 , which is TMUX1511 , if you are interested!
Regards
Saminah