Part Number: SN74GTLPH16912 Hi,
I am using SN74GTLPH16912 GTLP part design.
Can this part replace BTL transceivers because previous design using FB2030 part 5V compatible part.
New design using 3.3V logic peripheral planning to use this part.
…
Part Number: SN74GTLPH16912 Hi
I am planning to implement SN74GTLPH16912GR in one of our design.to convert from GTLP to LVTTL and vice-versa.
It is given in datasheet that VREF = 1V and VTT = 1.5V. Device has VREF pin but there is no VTT pin.…
Part Number: SN74GTLPH16912 the maximum rated operating temperature is given as 85 in the datasheet.
I am looking for the maximum rated junction temperature.
Please provide this value. Thanks
Part Number: SN74GTLPH16912 Hi
If I use the direction of SN74GTLPH16912GR from B to A, what would be the termination to be followed for control signals i.e, CLKAB, LEAB, OEABn and CEABn?
Regards
Srikanth Kacchu
Other Parts Discussed in Thread: SN74GTLPH16912
I have selected SN74GTLPH16912 as bus driver between mother board which has 16 backplanes and daughter board.
I have read some application notes at www.ti.com/gtlp but still have few questions:
…
Quickly find solutions to common questions about voltage translation (level shifter) devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
Auto-Bidirectional Level-Shifters
Fixed DIR / DIR…