Part Number: SN74HC00-Q1 Hi,
I am looking at gates that can work up to 140 degrees C operating for an automotive application.
Is there any device that can guarantee it? Or do we have any selection?
Our datasheets specify 125 degrees C max for all versions…
Part Number: SN74AC00 Other Parts Discussed in Thread: SN74HC00 , What gates/pins on SN74AC00 and SN74HC00 are ESD sensitive?
Also interested in ESD sensitive pin on the 74HC4051.
Thank you.
Found that the previously used ISO7241 digital isolators had internal 1Meg pull up resistors on the inputs. The ISO7341 used on this build (could not find any ISO7241 instock) do not have internal pull ups on the inputs therefore the outputs 2Y (EMU0…
Team,
Customer wants to know how much current the devcie can sink.
Being used in a control box and they want to put a watchdog timer in it. Testing for that purpose.
Thanks,
Aaron
Hi Clemens,
I also have some question about this Figure.
What does the output current and output voltage mean? Is it the SN74HC00 output?
What is the different for these two line?
Is the output current is the sum of 8 channles?
Why does the voltage can…
Part Number: SN74HC138 Other Parts Discussed in Thread: SN74HCS138 , , SN74HC00 , SN74HCS00 , SN74HCS139 Hello
do we have IBIS model for the SN74HC138NS, SN74HC139NS?
best regards,
kazusa suzuki
From the datasheets:
SN74HC00
50 mA
CD74HC00
50 mA
SN74HC374
70 mA
CD74HC374
50 mA
SN74AC00
200 mA
CD74AC00
100 mA
SN74AC374
200 mA
CD74AC374
200 mA
74AC16374
400 mA
It's not very consistent.