Part Number: SN74HC125 Other Parts Discussed in Thread: SN74AHC125 Tool/software: Provide the VIH, VIL, VOH, VOL Values for the respective IC at 3.3 VCC.
Part Number: SN74HC125
A buffer is currently used on the SPI bus, up to 5M speed, which acts as 5V converted to 3.3V. The buffer is 3.3 V supplied, the input is 5 V, and the output is 3.3 V, the circuit connections are approximately as follows:
…
Part Number: SN74HC125 Other Parts Discussed in Thread: SN74LVC125A , SN74LV125A , SN74AHC125 Hi,
Regarding the Switching Characteristics in the data sheet, is it possible to provide information when Vcc = 3.3V? Or please give me some reference information…
Part Number: SN74HC125 Other Parts Discussed in Thread: SN74HCS125 , SN74HCS541 , SN74HCS138
お世話になります
弊社製品の温度特性検査にて御社のICを使ってます
汎用 (general purpose) IC 74HC125、74HC138、74HC541
温度範囲はマイナス40度からプラス90度です (temp range is -40 to +90 C)
数年でICの交換が必要となる為…
Part Number: SN74HC125 Dear team
The customer fed ~3.3V to SN74HC125PWR as its supply voltage. According to datasheet, the V OH should really close to its V CC . However, we only got ~3.1V for the V OH by measurement.
We have tried to disconnect the…
Part Number: SN74HC125 Dear expert,
Customer use SN74HC125 in their application and face to VOH output voltage level issue.
They connect 3.3V for Vcc power supply, and measure output voltage is only 3.1V even there are no load connection at output…
Part Number: SN74HC125 Other Parts Discussed in Thread: CD4053B Hi Team
My customer is looking for 3 state buffer with below requirement.
Please advise recommended or close to the request devices.
1, Vdd > 6V
2, Output current > ± 50mA
Thanks…
Part Number: SN74HC125 Hi team,
Do we have the P2P solutions (SOIC package) that the direction from input to output is reversed? Thanks!
Best regards,
Sam Ting
Dear Emrys Maier,
Thank you for the quick reply.
As per the details mentioned, the SN74HC125 buffer is not suitable, since it can create issues in the design.
Our actual requirement is to interface two modules, out of which, any of the module…