Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: SN74HC139-Q1 Hi Team, My customer's application is Vcc=3.3V. I would like to ask about the following. 1) Is there VIH_min and VIL_max value under Vcc=3.3V? 2) Is there tpd_max (A or B to Y, notG to Y) value under Vcc=3.3V? Best Regards, Yaita …
Hi Kazuya
Kazuya Nakai59 said: Q1. How much is SN74HC139NSR ESD (MM, HBM, CDM) performance?
HBM: +/- 3 kV
CDM: +/- 200 V
We do not have MM ESD for this part.
Kazuya Nakai59 said: Q2. When I want to check ESD performance about other logics, do I need to ask…