Part Number: SN74HC165 Other Parts Discussed in Thread: SN74HCS165 , SN74LV165A , CD74HC165 , SN74HCS165-Q1 Is there p2p compatible one with new process as the Lead time of old one is not good? Pls recommend . Thanks
Part Number: SN74HC165 Dear,
the datasheet Note 2: When Vcc = 2V, Tt =1000nS =1000nS /V x (1.5V-0.5V) ? If Vcc=4.5V, Tt= 500nS/V x (3.15-1.35)=900ns, the chip will not be damaged. As long as it is below 1.35V or above 3.15V, it is safe?
If not, please…
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74HC595 , CD74HC299 , SN74LVC1G04 , SN74AHC1G04 Dear support team,
I am currently working at an GPIO extension for a microcontroller. I want to use 1 SPI Port for the extension with digital inputs…
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74AHC595 , Hi
I have a question to ask about the design of serial-to-parallel conversion design, which parts should be paid attention to, such as how to consider the bandwidth
Part Number: SN74HC165 Other Parts Discussed in Thread: CD74HC165 , , SN74HCS165 , ISO7740 Dear,
the datasheet Note 2: When Vcc = 2V, Tt =1000nS =1000nS /V x (1.5V-0.5V) ? If Vcc=4.5V, Tt= 500nS/V x (3.15-1.35)=900ns, the chip will not be damaged. As…
Part Number: SN74HC165
Hi teams
My customer used two pics SN74HC165 as cascaded configuration. According to datasheet guideline two device CLK should tie together.
I have a questions about time sequence requirement for device1 shift its data…
Part Number: SN74HC165
Hi All,
1. The customer would like to know the thermal metric(Θjc or Ψjt) and max Tj.
But we could not find it in the datasheet.
Could you kindly share those parameters with us?
2. And we would also like to know how…
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74HCT165 , SN74HCS165 Hi team,
Hope you're well!
My customer recently swapped out a SN74 LS 165AD for a SN74 HC 165DR on their board and are now experiencing failures where they weren't before…
Part Number: SN74HC165 Dear TI Experts
Can you help check the internal block of SN74HC165?
I'd like to know whether these three pins are connected to VCC internally:
CLK;CLK_IN;SH/LD